CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / CimClassDataItemExpression Json Schema
CimClassDataItemExpression Json Schema
Description
is a object to configure the expression attributes
Overview
CimClassDataItemExpression
is a object to configure the expression attributes
FirstOperandNum : number
is number that hlds the first (or left hand) side of the opperand if the value is to be treated as a number. Use CimClassDataItemExpression.FirstOperandString if your value is a string
FirstOperandString : string
is string that hlds the first (or left) hand side of the opperand. Use CimClassDataItemExpression.FirstOperandNum if your value is a number
ID : string
is a read only attribute that represents the ID of this expression
Operator : CimExpressionOperandTypesEnum
Specifies the browser type
SecondOperandNum : number
is number that hlds the first (or left) hand side of the opperand if the value is to be treated as a number. Use CimClassDataItemExpression.SecondOperandString if your value is a string
SecondOperandString : string
is string that hlds the second (or right hand) side of the opperand. Use CimClassDataItemExpression.SecondOperandNum if your value is a number
Properties
NameDescriptionData Type
is number that hlds the first (or left hand) side of the opperand if the value is to be treated as a number. Use CimClassDataItemExpression.FirstOperandString if your value is a stringnumber
is string that hlds the first (or left) hand side of the opperand. Use CimClassDataItemExpression.FirstOperandNum if your value is a numberstring
is a read only attribute that represents the ID of this expressionstring
Specifies the browser typeCimExpressionOperandTypesEnum
is number that hlds the first (or left) hand side of the opperand if the value is to be treated as a number. Use CimClassDataItemExpression.SecondOperandString if your value is a stringnumber
is string that hlds the second (or right hand) side of the opperand. Use CimClassDataItemExpression.SecondOperandNum if your value is a numberstring
See Also